Solution
Livestock Weighing System
A rancher wants to accurately weigh their cows for multiple reasons. They want to make sure their cows are at a healthy weight, and also want to maintain their weight.
A rancher wants to accurately weigh their cows for multiple reasons. They want to make sure their cows are at a healthy weight, and also want to maintain their weight. But they also want to know the optimal time for breeding based on the weight of their livestock.
Interface’s solution is to bolt four SSB Sealed Beam Load Cells at the bottom of a metal platform, that is placed on the inside of the customer’s cattle cage. Once the cow has walked onto the plate, the SSB Sealed Beam Load Cells will measure the force pressure applied. With all four connected to JB104SS Junction Box, which is then connected to the 480 Bidirectional Weight Indicator, combined accurate weight results will be displayed.
The customer was able to determine accurate weight measurements of their livestock in order to keep them healthy, or, to determine when was a good time to breed.